SELF-SANITIZATION AGAINST BACTERIA AND FUNGI
Understanding Sliding Friction in Industrial Design
May 16, 2023
Reading time: minutes
First, let's define sliding friction. Sliding friction is the force that opposes the motion of two surfaces sliding against each other. It is a type of kinetic friction, which means it only occurs when the surfaces are in motion relative to each other. This force is caused by the roughness of the surfaces in contact and the interlocking of the surface asperities otherwise known as abrasiveness. The force of sliding friction can be calculated using the coefficient of sliding friction, which is a value that represents the amount of friction between two surfaces.
Now, let's look at how sliding friction relates to Elesa's product offerings. Elesa is a global manufacturer of standard machine parts, such as handles, knobs, and leveling feet, that are used in a wide range of industries, including manufacturing, food processing, and pharmaceuticals. Many of our products rely on the science of sliding friction to function properly.
For example, Elesa's range of leveling feet relies on sliding friction to stay in place and support heavy loads. These leveling feet are made from materials such as stainless steel and technoploymer, which have different coefficients of sliding friction depending on the surface they are in contact with. By selecting the right material and surface finish for each application, Elesa's leveling feet can provide the necessary support and stability while reducing the force of sliding friction.

Another product offered by Elesa that relies on sliding friction is our range of cam levers. Cam levers are used to secure doors and panels in a wide range of applications, from industrial machinery to office furniture. The mechanism of a cam lever relies on the sliding friction between the cam and the cam follower to hold the door or panel in place. Elesa's cam levers are designed to provide the right amount of friction to hold the door or panel securely in place without damaging the surface.

Elesa's range of adjustable toggle clamps also relies on sliding friction to provide a secure hold. These levers are used to clamp objects in place and can be adjusted to provide the right amount of clamping force. The mechanism of the toggle clamp relies on the sliding friction between the clamping element and the object being clamped. Elesa's adjustable toggle clamps are designed to provide a reliable hold while minimizing the force of sliding friction.

In summary, sliding friction is a fascinating and important force that affects many aspects of our daily lives. It is a force that Elesa understands and incorporates into our product offerings to provide reliable and efficient solutions for our customers. By selecting the right materials and surface finishes, Elesa's products can reduce the force of sliding friction while providing the necessary support and stability.