SELF-SANITIZATION AGAINST BACTERIA AND FUNGI
Elesa Industrial Sight Glasses and Level Gauges
Sep 28, 2023
Reading time: minutes
This not only extends their lifespan but also reduces the need for frequent maintenance and replacements, saving both time and money.
Furthermore, Elesa understands the importance of customization in meeting the unique needs of different industries. For example, our level gauges can be tailored to meet specific requirements. This flexibility ensures that industries can find the perfect solution that fits their operations seamlessly.


Sight glasses are important for maintaining clear views of fluid levels in tanks, pipes, and vessels. In the world of industrial processes, maintaining a clear view of fluid levels is of the utmost importance.
Constructed from a transparent polyamide-based technopolymer, borosilicate glass, and many with a stainless-steel metal ring. Elesa sight glasses exhibit remarkable resistance to a multitude of challenges. These include shocks, solvents, oils with additives, and more. This exceptional resistance ensures longevity and reliability in diverse industrial environments.
A selection of our sight glasses are available with a prismatic window, which enhances the visual experience by bending light. This makes it easier to see fluid levels and processes more accurately.

A hydraulic level gauge, also known as a level indicator, is a device used to measure the level of a liquid in a container using a column of liquid in a vertical tube. It works on the principle of communicating vessels, where the liquid in the gauge's tube rises or falls to match the level of the liquid in the container.
The level of liquid being shown indicates the height of the measured liquid. This type of gauge is commonly used in industrial applications to monitor the level of liquids such as water, oil, or chemicals in tanks and vessels.
Distinctive Features of Elesa's Column Level Gauges
Elesa's column level gauges stand out because we put the level plate on the outside the gauge. By avoiding direct contact with the fluid, the coloration and readability of the level gauge remain unaffected. This design innovation ensures accurate and reliable visual monitoring without any compromise on clarity.
One of the key advantages of Elesa's level gauges with electrical sensors is their ability to prevent dry running. This occurs when a pump operates without sufficient fluid, leading to overheating and potential damage. By constantly monitoring the fluid levels, Elesa's gauges ensure that pumps are always operating within the optimal range, preventing costly repairs and downtime.
Empowering Industrial Pump Systems
Industrial pump systems play a pivotal role in various sectors. Our level gauges find a natural fit within these systems, offering insights into fluid levels. This proactive approach prevents pump damage, reduces maintenance costs, and ensures a consistent flow of operations.
As the hydraulic, lubrication, and industrial pump markets continue to evolve, Elesa's sight glasses and level gauges remain at the forefront of innovation. Our commitment to excellence and customer satisfaction has made us a trusted partner for industries worldwide.

Benefits That Define Excellence
Reliable Monitoring: Elesa's sight glasses and level gauges offer a reliable solution for fluid level monitoring. Their accurate measurements ensure that lubrication and pump systems operate optimally, minimizing the risk of downtime or operational disruptions.
Safety Enhancement: By offering clear visibility into fluid levels, Elesa's tank sight glasses and level gauges contribute to enhanced safety. Operators can proactively address potential issues, preventing overflows or inadequate lubrication that could lead to equipment damage.
Durable Construction: Constructed using robust materials, our sight glasses and level gauges are built to withstand the challenges posed by industrial environments. This durability guarantees a longer lifespan and consistent performance.
Compatibility: Elesa offers a diverse range of level gauge models that cater to various lubrication and pump setups. This ensures that we meet each system's unique requirements effectively.