SELF-SANITISATION AGAINST BACTERIA AND FUNGI
Elesa design: a success story exhibited at the ADI Design Museum
May 21, 2021
Reading time: minutes
The two Elesa mechanical components awarded with the Compasso d'Oro in 1994 will be exhibited in the Design Museum that will be inaugurated on May 25, 2021: the EWW. 240 manoeuvring handwheel with position indicator and the ECW. 375 manoeuvring handwheel from the Ergostyle® line.
Elesa manoeuvring handwheel with position indicator EWW. 240ADI Compasso d'Oro Award
The two mechanical components awarded the ADI Compasso d'Oro Award in 1994.
Visit the Elesa Design menu to learn more about the history!
New ADI Design Museum Milan
Elesa design at the new ADI Design Museum Compasso d’Oro in Milan.
Elesa's two mechanical components awarded with the Compasso d'Oro Award in 1994 will be presented at the Design Museum which will be inaugurated on May 25th 2021: EWW.240 handwheels for position indicators and the ECW.375 handwheels of the Ergostyle® line.
Elesa maneuvering handwheel with EWW position indicator. 240 ADI Compasso d'Oro Award
The awarded mechanical components by Compasso d'Oro Award in 1994.
Visit Elesa Design in order to find out more about the history!