SELF-SANITISATION AGAINST BACTERIA AND FUNGI
What makes an ergonomic industrial handle?
Jun 1, 2022
Reading time: minutes
What is ergonomics?
The philosophy behind ergonomics is that the fewer muscle groups needed to use a product, the more efficient it is to operate. This definition is difficult to apply to every person on the planet as we are wonderfully unique! Thankfully science has guidelines in the form of body measurement data called anthropometry. This data provides us with hand size percentiles on which to base our handle designs.
We supply parts for many industries and within those areas are many people with different body measurements. Thanks to Elesa expertise and anthropometry, our industrial handles are safe and comfortable for every one of your colleagues.
What factors should I consider?
The reason we supply so many types of pull handles are because they are useful for so many applications. As such, the ergonomic elements can vary between them. However, there are features that indicate that the principles of ergonomics are in play.
Shape
Our industrial door handles come in various styles, such as bridge, tubular, and bow. These are more ergonomic than standard doorknobs, which require a strong grip on a rounded surface and put a lot of pressure on the hand.
Elesa pull handles have rounded shoulders so there is no danger of sharp edges catching clothing or skin. Our handles are free from sharp corners and grooves, making them a safe and comfortable choice for any workplace.
The thickness of the handle is also an important factor in ensuring it is comfortable to hold. Too thick and it can be difficult to grip, too thin and the surface area can put pressure on the palm of the hand. Elesa industrial handles are produced in line with design parameters to deliver optimum ergonomics in whichever handle you choose.
Surface
Elesa industrial handles are made from quality metals such as steel and aluminium, as well as technopolymer – an innovative plastic with super strength and pleasing aesthetics.
These smooth but non-slip materials make operating the industrial handles extremely easy. They have also been thoroughly tested to ensure they are durable enough for heavy-duty use.
Why is an ergonomic handle important?
First and foremost, an ergonomic handle is important to reduce risk of injury and fatigue. Beyond this immediate benefit are other, perhaps surprising, advantages. Good ergonomics in the workplace can help staff be more efficient and productive, thanks to less exertion and energy spent operating poorly designed machinery. Consideration of ergonomics does not go unnoticed by colleagues. It shows a commitment to the happiness and wellbeing of your staff and in turn promotes a better safety culture, boosts morale, and strengthens company loyalty.
For Elesa, ergonomics is not just a buzzword. We know that the principle has real-world applications and can massively improve your workplace. Investing in Elesa’s specially designed components will provide immediate comfort for your workforce, and long-term dividends for your business.
EBP. Bridge handle, EPR-PF Flush pull handle, ETH Tubular handle