Header Header

TECHNOLOGY AND DESIGN

Established in 1941, ELESA is the international reference for standard components destined for the mechanical, machinery and industrial equipment sectors.

Historic Brand logo

An excellent combination of technology and design has given rise to a diverse production, thanks to the constant commitment to follow developments in engineering plastics and metal technology. A corporate culture strongly committed to product quality, combined with an innate sensitivity for design and ergonomic research, led to the creation of products unique and recognisable worldwide as ELESA products.

  • 300 PATENTS AND REGISTERED DESIGNS
  • 58 INDUSTRIAL DESIGN AWARDS
  • WORLDWIDE DISTRIBUTION
  • 80.000+ PRODUCT CODES AVAILABLE ON STOCK
  • CUSTOMISED SOLUTIONS
  • TECHNICAL COMPETENCE AT THE CUSTOMERS' SERVICE

Design and production activities are concentrated at the headquarters in Monza. An area of over 70,000 square meters, where tens of millions of pieces are produced every year by utilising the latest automated production technologies. In the new fully automated Logistics Centre, over 50.000 products are in stock and ready to be shipped worldwide.

ELESA uses electricity produced only from 100% renewable sources, i.e. energy produced through the use of natural resources (water, sunlight, wind, tides, geothermal heat, etc.) which therefore do not involve CO2 emissions (which are instead produced by coal, oil and gas).

QUALITY - ENVIRONMENT - SAFETY

Quality Management System certified according to ISO 9001

since 1993


Download the Certificate .pdf

QUALITY - ENVIRONMENT - SAFETY

Elesa UK - Quality Management System certified according to ISO 9001

since 1997


Download the Certificate .pdf

QUALITY - ENVIRONMENT - SAFETY

Environmental Management System certified according to ISO 14001

since 2007


Download the Certificate .pdf

QUALITY - ENVIRONMENT - SAFETY

Occupational Health and Safety Management System certified according to ISO 45001

since 2012


Download the Certificate .pdf

QUALITY - ENVIRONMENT - SAFETY

Authorised Economic Operator Full certified by the European Custom Agency

since 2014: recognition of full reliability of customs procedures


Check the status of AEO Elesa (Authorised Economic Operator)

QUALITY - ENVIRONMENT - SAFETY

Information Security Management System certified according to ISO 27001

since 2024


Certificate download .pdf

ELESA is associated with:

THE UTMOST COMPETENCE

ELESA continues to invest in R&D, and in particular, the innovation of its production technologies, with the aim of creating new products or to further improve performance and reliability of existing ones.

An internal testing laboratory with the most advanced equipment and measuring instruments, studies the evolution of new plastic materials to develop new and improved products, satisfying the requirements of more demanding applications in the field of industrial machines.
All standard products in the ELESA range are subjected to mechanical, physical, chemical and durability testing in order to provide correct and reliable technical data.
The ELESA laboratory is at the disposal of customers for carrying out tests that simulate specific or particularly heavy conditions of use.

Go to Elesa Youtube channel to find out more about laboratories tests!

CUSTOMISED SOLUTIONS

In addition to the widest range of standard machine elements available on the market, ELESA offers on demand customised technical solutions to meet the customer's specific needs. Production flexibility, technical know-how, R&D, constant activity and customer care allow for quick answers and competitive solutions.

PRODUCT CUSTOMISATION
Logos and text by tampoprinting, laser-engraving and moulding
SPECIAL COLOURS
Non standard colour options
SPECIAL MATERIALS AND SHAPES
Special technopolymers, stainless steel and metals; special shapes, dimensions and metal inserts
SURFACE TREATMENTS
Black-oxide coating, zinc-plating, nickel plating, chrome-plating, anodising, epoxy-resin coating