SELF-SANITISATION AGAINST BACTERIA AND FUNGI
Hygienic Design Standard components
Sep 28, 2023
Reading time: minutes
Typically, most components and accessories installed on machines and industrial equipment in these environments seem to be sufficiently distant from the critical work areas, but airborne spores of microorganisms are able to spread quickly and to distant surfaces. So even the smallest corner can be the start of contamination across a complete production line.
Hygienic Design line consists of a range of standard components that offer the possibility of achieving optimal levels of hygiene with a minimum degree of probability of contamination, and compliance with very high standards in sanitary matters such as 3-A, EHEDG and DGUV guidelines.
In addition to the more traditional components such as handles, handwheels, knobs and clamping levers, levelling feet, including nuts and screws, today the "Hygienic Design" range is enriched with lever latches, indexing plungers and spacer sleeves.
There are different types of AISI stainless steel used for different types of components, from AISI 316L to 30,4 including CF8, with different surface finishes: sandblasting mat or polished surfaces with maximum surface roughness that remains below Ra 0.8 μm so that dirt particles cannot settle and can be reliably removed during cleaning.
Also particularly important are the H-NBR or EPDM synthetic rubber seals, FDA-compliant, which allow the internal part of the mechanism to be sealed from the external environment, preventing the access of substances. Absence of cavities and recesses and geometries with large corner radii prevent adhesion of impurities and facilitate cleaning operations.
The sealing gaskets in H-NBR and EPDM elastomer were tested using simulation software to ensure the retention of the degree of hygiene after assembly, demonstrating that they perfectly adhere to the surfaces and therefore fulfil their function long term.
The components of the "Hygienic Design" line facilitate cleaning operations which can be carried out faster via the "Clean in Place" concept with long-term impacts on the efficiency level of the entire system.