SELF-SANITISATION AGAINST BACTERIA AND FUNGI
How to use adjustable feet
May 23, 2022
Reading time: minutes
What to use adjustable feet for
Adjustable feet can also be used on equipment to reduce sliding, tipping, vibration, and general wear and tear. Not only does this make your work environment safer, but it also extends the life of your machine to save money in the long run. When choosing levelling feet, you must consider the needs of your work environment. You may require mountable, heavy-duty, or other types of adjustable feet. Below we will explain how to make the best choice.
Assembling and installing adjustable feet
Adjustable feet come with a threaded screw, of which we provide many sizes. These solid stems are made from quality steel to ensure your equipment remains safe and secure.
To install levelling feet, use the threaded screw to affix the components to your machine. Once the thread is securely fitted, you can adjust the height of the levelling feet by loosening or tightening the threaded shaft.
Types of adjustable feet
Alongside standard machine feet, we provide components with additional features to meet your needs.
Adjustable feet for ground mounting
Our mountable levelling feet feature special knurling on the lower lip of the base to allow it to stand flush against the floor. For simple affixing to the ground, the feet come with two pre-drilled holes at 180˚. The holes are covered by a removable diaphragm to protect the base from debris of dust and dirt when the feet are not mounted.
LV.F , LVQ.F-SST, LV.FO, LV.F-125-AVC
Adjustable feet with no-slip properties
There will be situations where mounting machinery to the ground is not suitable, but it is still imperative that your equipment remains safe and stable. For these purposes, we provide levelling feet finished with no-slip disks.
We have performed thorough tests of separation to ensure that our no-slip levelling feet deliver the required support for your equipment. Our specially designed disks provide a perfect anchoring which prevents separation even during transportation.
Accessories for adjustable feet
As well as levelling feet, we also provide accessories to use with the components. Our accessories include the following:
Screws and nuts with hygienic design
Certified by the European Hygienic Engineering and Design Group, these stainless-steel components are ideal for use in environments that require a high level of hygiene. They come in a matte or polished finish and with a choice of packing ring.

End caps for tubes
Our range of end caps can be used to cover the rough-cut end of a metal profile. We supply end caps in square and round.

NDX.Q, NDX.T, STC, NIL, NCT, NCD
Bases, nuts, and stems
As well as complete adjustable feet, we provide packs of individual bases, nuts and stems so you can create the perfect component for you. Just like our standard levelling feet, these products are made from quality materials such as technopolymer and stainless steel. For help with matching stems with bases, consult the Elesa catalogue.
SM., SMQ-SST, bases LS.A - LV.A - LV.F