ITSESTÄÄN PUHDISTUVAT OSAT BAKTEERIEN JA SIENIEN TORJUMISEKSI
Push button
Generally it is the point pressed by the operator’s thumb to lift the lever. Technopolymer adjustable handles are generally equipped with a technopolymer push button.
Among other things, this provides a total electrical insulation for the operator.
The push button in ERX. models is available in the six ERGOSTYLE colours.
Models with a metal clamping element have got a hexagonal socket screw for lever disassembly or quick screwing by means of electric or pneumatic tools. Quick screwing can also be done with the ERX.AV, technopolymer version, using the six-lobe socket (TORX® *) located in the technopolymer clamping element.
*marque enregistrée par TEXTRON INC.